Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the minimum version of firmware required for the CM4000 and CM3000 to enable the Harmonic Power Flow calculations?

Issue
Harmonic Power Flow Calculations will not be performed on firmware versions below a certain revision.

Product Line
CM3000
CM4000

Environment
Harmonic Power Flow Calculations
Firmware

Resolution
It is necessary to have CM4000/3000 firmware version 12.32 or later to enable the Harmonic Power Flow calculations.

Access to firmware upgrade instructions, including a how-to video and a link to the latest firmware can
be found at: Firmware Upgrade - Instructions and Downloads

Additionally, supporting documents and file downloads on this and a wide variety of other products and topics
may be obtained using the search function found at the: Download Center