Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Running Designer on a client machine reports an error when trying to open a node diagram

Issue

Opening a meter node template in Designer on a newly installed client machine reports the following error "The directory for node diagram could not be created"

Node message

Product Line

Ion Enterprise 5.x/6.x
Struxureware Power Monitoring Expert 7.0.x
Struxureware Power Monitoring Expert 7.2.x Base/Healthcare/ Data Center Edition
Struxureware Power Monitoring Expert 8.0 Base/Buildings/Healthcare/ Data Center Edition

Environment
Open meter template in designer

Cause
1) The sharing permissions of the ION_Ent share folder are not set properly on the primary server
2) The client machine's Root2 registry key is not pointing to the config folder on the primary server

Resolution
1) To resolve the issue, please follow the below steps:
1. On the primary Ion Enterprise/PME machine navigate to the folder Ion Enterprise/Power Monitoring Expert folder. The paths are as below:
For Ion Enterprise 5.x/6.x machines :                            ..\Program Files\Schneider Electric\
For SPM7.x/PME7.2.x/PME4DC7.2.x/PME4HC7.2.x/PME8 (all editions) : ...\Program Files (x86)\Schneider Electric\

2. Right click on Ion Enterprise/Power Monitoring Expert folder and go to properties and then click on tab labeled "Sharing"

Sharing proeprties

3. Click on "Advanced Sharing" which will open a new window. Click on permissions

Advanced sharing

4. In the share Permissions tab, select Everyone on the top and provide permission to "change" by checking the box to Allow.

Permissons

NOTE:
All share permissions are automatically set to the Read permission for the Everyone group; this includes the ION Enterprise share (ION_Ent).
A user must configure the ION_Ent share to the Change permission only if installing Secondary Servers on the network or if installing Clients
that require more than just Read permissions (e.g., A client user need to Modify Vista diagrams, update device templates etc)

2) Follow the steps below to check the value of the Root2 registry key on the client machine and ensure it is pointing to the config folder on the application server:

** Warning - Making registry changes can render the operating system inoperable.  If you have any questions or concerns over this procedure please contact Powerlogic technical support at 615-287-3400 for assistance. **

1.  On the client machine type 'regedit' into the Windows start menu search.
2.  Right click on 'Computer', select the Export option, and save this file in a secure location.  This will create a full back up of the registry in case any changes need to be reverted.
Registry export

3.  Browse to the registry directory below depending on the software version installed.

PME 7.2 and newer - Computer\HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Schneider Electric\Power Monitoring Expert\(version number)
PME 7.0.1 and older - Computer\HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Schneider Electric\ION Enterprise\(version number)

For example, the full registry path for a PME 8.1 system would be:

Computer\HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Schneider Electric\Power Monitoring Expert\8.1

while an ION Enterprise 6.0 system would be:

Computer\HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Schneider Electric\ION Enterprise\6.0

4.  Within the numbered directory locate the 'Root2' registry key.  On a client machine this path will point to the primary server's config folder. (example: \\PMESERVER\ION-Ent\config).  On the server itself the path will display the local config directory as seen in the screen shot below.

Registry editor

5.  Update the path in the Value data field after double clicking the 'Root2' registry key.
String edit