Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How do I download/copy a waveform from ION Setup?

Issue
A user may want to copy a meter's waveform from ION Setup into Excel.

Product Line
ION Setup 3.0

Environment
ION Setup Waveform Log
Microsoft Excel

Cause
The user wants to copy the waveform logs generated in ION Setup.

Resolution
Once in ION Setup Software, navigate to Data Screens>>Waveform Log and open the desired waveform(s). Follow this procedure to copy the waveform data and paste it into an Excel document:

1)  Click on the desired waveform label (see below).
2)  Open the Edit menu and choose 'Copy'.
3)  Open Excel and paste data in a new spreadsheet.

This will paste the raw data, which you will then be able to re-graph sections or the whole graph in your preferred graph type.

ion setup

See video below for an example: