Issue
What are the control power requirements for the ENA?
Product Line
Enercept Meter, ENA
Cause
User would like to know control power range for ENA
Environment
Installing ENA
Resolution
The control power requirements for the ENA (Enercept Network Adapter) are as follows: 9-30Vdc or 12-24Vac ; not including power factor, 1.5W max, 125mA max @12Vdc, 65mA max @24Vdc.
Released for:Schneider Electric Saudi Arabia