{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What does AMPS OVER represent on the display of an Energy Meter?

Issue
AMPS OVER displayed on Energy Meter

Product Line
EMBxxxx, EMExxxx, EMHxxxx

Environment
Front panel display

Resolution
If the measured current is greater than 110% of the rated CT range, the display will show AMPS OVER and indicate the specific phase(s).

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.