Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
[OID]Reset=1 does not reset OIDs when tags are in an include project

Goals and Symptoms

Summary:
It was found that setting [OID]Reset=1 in the Citect ini file, did not reset the OIDs when the variable tags are located in an include project.
I've used Open Office to modify my variable.dbf.

This behaviour also exists when using the ProjectDBFAddIn macro with the 'Save Only" option.
Using the "Save and Reindex" option however allowed the OIDs to be reset

I'm able to reset without any problems if the variable tags are located in the main project after I've modified the variable.dbf using
- Open Office
- ProjectDBFAddIn macro with the 'Save Only" option

Facts and Changes

Keywords:
OIDs, OIDs do not reset, Open Office, ProjectDBFAddIn, [OID]reset=1

Causes and Fixes

Solution:
- Have the variable tags in the main project if you are using
- Open Office
- Use the ProjectDBFAddIn macro with the "Save and Reindex" option


Ctiect is aware of this problem and we are currently investigating this issue.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre