Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
MODNET string variable configuration

Summary:

I have configured a string variable communicating to a PLC via MODNET and I can only see the first 2 characters of the string. How can I see the whole string?

Solution:

If you specify a string tag with the address 40001, the MODNET driver will only read register 40001 (2 bytes so 2 characters). If you want a string longer than 2 characters you have to create your tag as an array of characters so the driver knows how long the string is. So if you want a string of length 10 you need to setup an array of length 5. image


Keywords:

MODBUS

________________________________________