Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the range of value that Arithmetic module supports in VIP ?

Issue
User would like to know the range of value that Arithmetic Module supports in VIP (Designer)?

Product Line
ION Enterprise, StruxureWate Power Monitoring Expert 7.0.1, PME 7.2.x, PME 8.x

Cause
User would like to know the maximum and minimum range supported with Arithmetic Module within VIP.

Resolution
For Arithmetic module in VIP, the data type of the output register is 64 bit floating point. Therefore, it allows a range from -10 ^ 308 to +10 ^ 308.