Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ION 8650 Communication Field Retrofit Kit

Issue
A customer would like to order a communication field retrofit kit for the PowerLogic ION 8650 meters and requires installation instructions.

Product Line
PowerLogic Revenue Meters

Environment
PowerLogic ION 8650 meters

Cause
Customer is looking to modify the integrated communication card feature set on an ION 86XX meter. Instructions for field retrofitting the meter are required.

Resolution


ION 8650 Field Retrofit Communication Cards:

Part NumberDescription
FR-8650-C78650 Full Communication Card FR Kit
FR-8650-E18650 Ethernet Communication Card FR Kit
FR-8650-M18650 Modem Communication Card FR Kit

Refer to the PowerLogic ION8650 Field Retrofit Instructions for steps on replacing the communications card.

Schneider Electric Saudi Arabia

Attachment(s)
PowerLogic ION8650 Field Retrofit Instructions.pdf [2.41 MB]