Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
StruxureWare Power Monitoring 7.0 - Why do I see 'an unexpected error has occurred' when I try to add a Report Subscription in Web Reporter?

Issue


IfStruxureWare Power Monitoring 7.0 is installed as a distributed system (both a database server and an application server) and Reporting Services is installed on the database server, you will not be able to create a report subscription. When an attempt is made to add a report subscription, in the Web Reporter UI, the user will see a screen that says ''unexpected error has occurred. Your request cannot be processed at this time. If the problem persists, contact the Webpage administrator'.

If you look in the EventException table, the following will be displayed:

System.ApplicationException: Could not authenticate. at PowerMeasurement.Security.UserImpersonator..ctor(String username, String password, String domain) at PowerMeasurement.Apps.Web.EEM.Modules.Reports.AddRSReportSubscription.InitPrinterControl() at PowerMeasurement.Apps.Web.EEM.Modules.Reports.AddRSReportSubscription.Page_Load(Object sender, EventArgs e) at System.Web.Util.CalliHelper.EventArgFunctionCaller(IntPtr fp, Object o, Object t, EventArgs e) at System.Web.Util.CalliEventHandlerDelegateProxy.Callback(Object sender, EventArgs e) at System.EventHandler.Invoke(Object sender, EventArgs e) at System.Web.UI.Control.OnLoad(EventArgs e) at System.Web.UI.Control.LoadRecursive() at System.Web.UI.Page.ProcessRequestMain(Boolean includeStagesBeforeAsyncPoint, Boolean includeStagesAfterAsyncPoint)

Product Line
StruxureWare Power Monitoring (SPM) 7.0 or 7.0 to 7.0.1 Upgrade

Cause
This problem results because the IONUser windows account is not created on the application server at install time.

Resolution
The workaround is to add the IONUser Windows account manually. The password should be set to 'IONisgreat!' without the single quotes.. Most of the time, It does not need to be a member of any group. However, if the same error message shows up again, adding the IONUser to the Administrators group can correct the error.

This problem has been addressed in Struxureware Power Monitoring 7.0.1, but only on new installations. SPM 7.0 systems that are upgraded to SPM 7.0.1 will need to have the IONUser added to the application server manually.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre