Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to display a Setup Register value on the front panel display screen?

Issue
By default, the data shown on the meter front panel display screen is determined by the links to the display modules Source inputs. The Source inputs of the display module can typically be linked to the output registers of other modules so as to allow data flow from one module to another. Customers may want to display the values from setup registers on the front panel screen, creating custom displays.

Product Line
ION7300
ION8600
ION8500
ION8800
PM8000
ION7550/ION7650
ION7500/ION7600
ION9000

Resolution
this can be accomplished via either ION Setup or Designer
ION Reference (module guide): ION Reference Home (se.com)

ION Setup

  1. Follow these directions for ION meter setup: How to add a device into ION Setup | Schneider Electric USA
  2. Open the Setup Assistant for your meter. See the ION Setup Help for instructions.
  3. Select the Displays screen.
  4. Select Displays on the Front Panel tab and click Edit.

    ION Setup uploads your meter’s display information to the Display Editor. This can take a few moments.

  5. Edit, rename, delete or rearrange displays as needed.
  6. Click New to add a new display or click Edit to change an existing display. The Display Setup wizard appears. There are three basic steps for creating or editing display screens.
    1. Select a Screen Type: Choose the screen type you want from the dropdown list.
    2. Select Parameters: Link or unlink the parameters available for your chosen screen type. Assign your preferred display units (if required); see Considerations when assigning display units for considerations and examples of display unit scaling.
    3. Select Digit Display Properties: Select your display qualities, including digit resolution and truncated or rounded last digits.
  7. Click Send to save the changes in the meter.


Designer

If you want your new screen to appear in the automatic scrolling cycle, you must link the Show input of the Display module to a Trigger output of a Scroll module.

  1. Create a Display module.
  2. Define the modules characteristics (display format) by adjusting its setup registers.
  3. Link any required data to the Source inputs of the Display module.