Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the mounting brackets used to mount Powerlogic Split Core Current Transformers (SCCTs), Energy Meter CT's, or Enercept Meters?

Issue
A user may want to find the part number and dimensions for the mounting brackets

Product Line
Current Transformers

Environment
Power Monitoring and Metering

Cause
There may be a need for current transformers to be mounted and affixed inside a current transformer cabinet or gutter. Mounting them requires more space but makes the installation cleaner, more orderly, and easier to troubleshoot regarding potential future issues.

Resolution
*Warning: Installation and maintenance of this device should only be performed by qualified, competent personnel that have appropriate training and experience with high voltage and current devices. Failure to follow the instructions / warnings in the Meter Installation Guide can result in permanent damage to the meter, severe injury or death.

The part number for the mounting bracket for the PowerLogic Split Core Current Transformers (SCCT) is 3050EMBK3.
NOTE: this part number comes in sets of three.

The mounting brackets are the same as those used to mount the PowerLogic Energy Meter CT's and Enercept Meter CTs, but will also fit all ratings of the PowerLogic Split Core Current Transformer.

1