Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which Modbus Commands are supported by PM7 and PM8?

Product Line
PM710
PM750
PM800 Series

Environment
Modbus Commands

Resolution
The following modbus commands are supported by PM710
PM710 Commands
*Reference page 36 of the PM710 Reference Manual .

The following modbus commands are supported by PM7​50
PM750 Commands
*Reference page 48 of the PM750 Reference Manual .

The following modbus commands are supported by PM8
PM800 commands
*Reference page 81 of the PM800 User Guide attached.

Schneider Electric Saudi Arabia

Attachment(s)
PM800-User_Guide.pdf [3.42 MB]