Issue:
Pulse width output
Product Line:
ION6200
Environment:
ION 6200
Cause:
Time Constant, kT, is the number of units (kWh,kVah,kVARh) per output transition.
Resolution:
The digital output uses KY pulsing. This means that the relay changes from open to closed or from closed to open whenever kT units have been measured (20 transitions/second maximum).
Released for: Schneider Electric Saudi Arabia