Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can different compression ratios be applied to the length and the width of the diagram when using the "Fit to Window" option in PME Vista?

Product Line:
Power Monitoring Expert (PME)

Environment:
PME Vista

Resolution:
Vista will automatically reduce and increase the diagram size by the same ratio in order to maintain the scale before pressing "Fit to Window." Vista maintains the aspect ratio in order to prevent stretching, but if the items are stretched before pressing "Fit to Window" they will scale with the new dimensions.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre