Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the RJ11 Pinout for the 6200 TRAN Meter?

Below is the pinout for the 6200 TRAN RJ11 Connector for the Modular Display:

Pin 1: Vcc
Pin 2: GND
Pin 3: -Signal
Pin 4: +Signal
Pin 5: GND
Pin 6: Vcc




Last Revised: September 21, 2007
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL188295 V1.0, Originally authored by KBAdPM on 10/04/2007, Last Edited by KBAdPM on 10/04/2007
Related ranges: ION6200

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre