Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ION Setup gives 'Unrecognized Serial Number' Error

Goals and Symptoms

Summary
ION Setup will display an error message if the incorrect serial number was used during installation or if the serial number was changed after installation.
All installations of ION Setup should use the same serial number (0409-0001-102-3574).

Symptoms

When starting ION Setup, the following error is displayed:


Error reads:

  • Unrecognized Serial Number.
    Execution halted.

Causes and Fixes

CauseThis error is likely caused by the user entering their ION Enterprise serial number for ION Setup during installation.

Resolution

  1. Open the Registry Editor
    1. Click Start > Run...
    2. Type regedit and click OK
  2. Expand HKEY_LOCAL_MACHINE > SOFTWARE > Schneider Electric > ION Setup > 2.1, as seen below

  3. Edit the SerialNumber key, and change it to the corrent serial number for ION Setup

    0409-0001-102-3574
  4. Close the Registry Editor
  5. Re-run ION Setup



Last Revised: October 15, 2007
Public
All content © 1992-2007 Schneider Electric

Legacy KB System (APS) Data: RESL188495 V1.0, Originally authored by KBAdPM on 10/17/2007, Last Edited by KBAdPM on 10/17/2007
Related ranges: ION Setup 2.1

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre