Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
WebReach Diagram Displays 'WebReach Default Diagram Node'

When viewing a custom diagram in WebReach the text 'WebReachDefaultDiagramNode' is displayed under all/some objects, but this label is not shown when the diagram is viewed in Vista.

  • Web reach

Resolution
  1. Open the diagram in Vista
  2. Select all the objects that are displaying this problem.
  3. Right-click on one of the objects.
  4. In the Caption tab, change the Caption selection from Use Default to None.
    Configuration
  5. Save your changes and reload the diagram in WebReach