Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do ION meters encrypt data transmitted in the ION protocol?

Product Line
ION Meters

Environment
Encryption

Resolution
The ION meters do not and cannot provide data encryption. The data from the ION meter is "cryptic", however, in the sense that one would need to understand the ION protocol in order to interpret the data.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre