How can we help you today?

WebReach can display real-time data but can't display Objects

WebReach can not display objects, however real time data can be displayed. The possible cause might be a missing dll file called ImgX61.dll which runs under WebReach engine to display objects. It can be located on the install disc. Copy the file into .../ION Enterprise /system/bin and register it:
1. Open a CMD prompt and navigate to .../ION Enterprise/system/bin
2. Register imgx61.dll by typing:

regsvr32 imgx61.dll

3. Exit the CMD prompt




Last Revised: November 13, 2007
Applies To: WebReach
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189170 V1.0, Originally authored by KBAdPM on 11/14/2007, Last Edited by KBAdPM on 11/14/2007
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5

Schneider Electric Saudi Arabia