Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Event Timestamps in Management Console Show in UTC Time Instead of Local Time

Issue
Event Timestamps in Management Console are displayed in Coordinated Universal Time (UTC) rather than in local time. Adjusting the server time zone in Windows settings has no effect on the timestamps.

Product Line
ION Enterprise
Power Monitoring Expert (PME) 7.x
Power Monitoring Expert (PME) 8.x
Power Monitoring Expert (PME) 9.x
Power Monitoring Expert (PME) 2020
Power Monitoring Expert (PME) 2021
Power Monitoring Expert (PME) 2022
Power Monitoring Expert (PME) 2023
Power Monitoring Expert (PME) 2024

Environment
Power Monitoring Expert (PME) Management Console

Resolution 1: Older Versions
A timestamp setting in Management Console is not configured correctly.

  1. Open the Event tab under Devices or Sites, whichever is showing UTC time.
  2. Right-click the grey section in the title bar and select Properties.
  3. Select the Row Properties tab from the Option window.
  4. Check the Convert timestamps to local date and time box.
old management console screen

Resolution 2: Newer Versions

  1. Open Managment Console
  2. Click on Tools > Options
  3. Make sure the box for "Convert Timestamps to local date and time" is selected
new options section in management console

All timestamps will now be displayed in the local time zone of the computer running Management Console.

NOTE: This setting is applied to all Event timestamps.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: