Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
License Manager - ActiveX component can't create object error message

Goals and Symptoms

The following error message is displayed when the License Manager is opened from Management Console:
License key error screen
Error reads

  • License Manager
    ActiveX component can't create object

This error also appears when you go to Management Console > Help > About

Causes and Fixes

Cause
The cause of the problem is when the "About" or the "License manager" tries to retrieve ProductInfo.edition. This value is constructed by ProductInfo from the license key.

Resolution
The IONSNG.dll must be re-registered:

  1. Open a CMD prompt and navigate to ...ION Enterprise\system\bin
  2. Type the following to re-register the .dll:
    regsvr32 ionsng.dll
  3. A confirmation window should appear

    Message reads
    RegSvr32
    DllRegisterServer in ionsng.dll succeeded.
  4. Ensure that Imgx61.dll exists and re-register it as well following the same procedure

NOTE: The above re-registering will resolve the problem, but in case it does not work, try running a Repair on the installation to make sure all dlls exist and are registered properly.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre