Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are all ION 7650s Conformal Coated? If not, can they be ordered as such?

Issue
Are all ION 7650s Conformal Coated? If not, can they be ordered as such?

Product Line
ION 7650 Power Meters

Environment
ION 7650 meters, ordering options, environmental protection

Resolution
Conformal coating material is applied to electronic circuitry to act as protection against moisture, dust, chemicals, and temperature extremes that, if uncoated (non-protected), could result in a complete failure of the electronic system. The coating material can vary depending on conditions. For more information, refer to the following link:
http://en.wikipedia.org/wiki/Conformal_coating

Schneider Electric's "Tropicalization" process is a conformal coating of silicon spray. This option is not standard; it is optional. To have the meters prepared with a conformal coating, the "Tropicalization" order option must be requested from the "Special Order" section of the order form.