Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the power supply of a 6200 meter operate over 480VAC?

From the design perspective of the 480V power supply, any voltage greater then 480V pushes the limits of the power supply. If it is desired to provide an input slightly above 480VAC (i.e. 495VAC RMScontinuous) it may reduce the lifetime of the power supply and is therefore not recommended.

Last Revised: November 22, 2007
Applies To: ION 6200
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189537 V1.0, Originally authored by KBAdPM on 11/23/2007, Last Edited by KBAdPM on 11/23/2007
Related ranges: ION6200