Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can one use ION Setup to connect an ION6200 meter in single device mode?

Issue
User would like to use ION Setup to connect to an ION6200 meter in single device mode

Product Line
ION6200

Environment
ION Setup

Resolution
No, ION Setup cannot connect to an ION6200 in Single Device Mode. Network Mode is required.

  1. Right click > Insert Item > Group
  2. Select the created group
  3. Right click >Insert Item > Site
  4. Configure the Site (Serial/Ethernet)
  5. Right click > Insert Item > Meter
  6. Configure the ION6200 meter
  7. Click OK

You should now be able to double click the meter and access its modules.