Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When creating a custom map for importing OPC data into ION Enterprise, is it possible to add control setup, boolean setup, and scaling within the translator file?

The ION Enterprise OPC Client feature does not support anything except reading real time values. An alternative solution would be to use the VIP to add additional functionality. An arithmetic module can be used to add scaling and a convert module can be used to create a boolean register.

Date Created: February 25, 2009
Last Revised: April 29, 2009
Public
Original Author: MN
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL198403 V1.0, Originally authored by MiNe on 04/30/2009, Last Edited by MiNe on 04/30/2009
Related ranges: ION Enterprise V5.6

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre