Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ION7650 or ION7550 meter gives Error 195 on the front panel

Issue
Error 195 appears on the front panel of an ION7650 or ION7550 meter

Product Line
ION7650

ION7550

Environment
HMI of meter

Resolution

If Error 195 appears on the front panel of an ION7650 or ION7550 meter, upgrading the firmware to version (v352) or later will resolve this issue.