." | Schneider Electric Saudi Arabia" />

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ION Enterprise v5.6: Meter M@il Archiver warning appears in the Windows Application Event Log: "The current size (size MB) of ION_Data database has passed its maximum allowed size (5000 MB) on server <server name>."

There is a <MaxSizeMB> value specified in the Metermailcfg.xml file normally located in the MeterMailArchiver\config directory. The default is 5000 MB. Increasing the value to something much larger (like 50000 MB) will get rid of the errors.

Date Created: November 4, 2008
Last Revised: May 1, 2009
Public
Original Author: MN
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL198416 V1.0, Originally authored by MiNe on 05/02/2009, Last Edited by MiNe on 05/02/2009
Related ranges: ION Enterprise V5.6