Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Deactivate Communication Error Alerts for Nodes in Vista.

Issue:


Customer would like to know how to deactivate nodes or suppress “Communication Error” alerts for devices that are known to be deactivated or have known issues.



Error Message



Product Line:

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024



Cause:

User receives “Communication Error” for nodes that are not responding. These may be deactivated meters or devices with known issues, and the user wants to prevent Vista from displaying these alerts.



Environment:


Vista showing "Communication error" in Vista



Resolution:


Log into ION Enterprise Vista and click on "Options". Here is two options:


1.  User can "Uncheck" the "Alert on Comm errors for Disabled Devices" which will not give "Communication error" for deactivated devices.
2.  User can "Uncheck" the "Alert on Comm Errors" which will deactivate the "Communication error" for all devices.


"Uncheck"

Recommendation:

If you are using an older version of PME, consider upgrading to the latest version for improved protocol support and security. For assistance with integration or upgrades, contact Schneider Electric Technical Support at: pmo-psup@se.com

Support details