Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How Does Tenant Metering Software Commercial Edition (TMSCE) Calculate 15, 30, or 60 Minute Rolling Demand?

If the data is collected on a 15 minute interval, there is no difference between rolling demand and present demand. Data that is collected on a 5 minute interval is the average of the current interval and the previous two. For example, if the data is measure at 2:00, 2:05, 2:10, 2:15, 2:20, 2:25, and 2:30, the rolling demand for 2:20 would be the average of the readings taken at 2:10, 2:15, and 2:20.
With 15 minute interval data, the 30 minute rolling demand is calculated by averaging the previous demand interval with the current one. For example, data is taken at 2:00, 2:15, 2:30, 2:45, and 3:00. The 30 minute rolling demand for 2:45 is the average of the demand readings at 2:30 and 2:45.

With 15 minute interval data, the 60 minute rolling demand is calculated by averating the current demand interval with the previous three. For example, data is taken at 2:00, 2:15, 2:30, 2:45, 3:00, 3:15, 3:30, and 3:45. The 60 minute rolling demand for 3:15 is the average of the demand readings at 2:30, 2:45, 3:00, and 3:15.


Legacy KB System (APS) Data: RESL198518 V1.0, Originally authored by AnVa on 05/16/2009, Last Edited by AnVa on 05/16/2009
Related ranges: Tenant Metering Software