Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do PowerLogic and ION meters use DHCP to dynamically determine an IP address?

Issue
Do PowerLogic and ION meters use DHCP to dynamically determine an IP address?

Product Line
PowerLogic
ION

Environment
Communication Protocols

Resolution
With the exception of the E4800, EM4800, PM55XX, PM8000 and ION9000 meters, PowerLogic and ION Meters do not have DHCP capability.