Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between an EGX100 and a TSXETG100?

Issue
What is the difference between an EGX100 and a TSXETG100?

Product Line
EGX100

Environment
Part number

Cause
Are different protocols supported between the EGX100 and TSXETG100?
Do the EGX100 and TSXETG100 support the same devices?

Resolution
The EGX100 is a Square D branded Ethernet gateway and the TSXETG100 is a Telemecanique branded Ethernet gateway. The units are physically the same, but offer different transmission modes for serial communications.
The EGX100 supports Modbus RTU, Jbus, PowerLogic (SY/MAX), and Modbus ASCII.
The TSXETG100 only supports Modbus RTU and Modbus ASCII. PowerLogic legacy devices such as CM100/200s and CM2000s, as well as SEPAM Relays, would be unable to communicate through a TSXETG100.