Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will the ION8600, ION7650, and ION7550 modems work with a digital modem line that is run through a multiplexor.

Issue
Will a multiplexor work with digital modem lines

Product Line
ION7550
ION7650
ION8600

Environment
Communications

Resolution
There are no known issues with an ION meter's modem working with a digital modem line that is run through a multiplexor. As long as the multiplexor transmits packets completely then there should be no problem.
The digital modem is normally supposed to be made to work with analog modem, so this should not be an issue. It is important to ensure that the ION8600 meter is receiving an analog signal, as it will not work with a digital signal.