Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will the P765CA0A COMM card work on legacy ION7500/7600 meters?

Issue:
Can a P765CA0A communications card for the ION 7550 / 7650 meter be used in an older ION 7500 / 7600?

Product Line:
ION7500
ION7600
ION7550
ION7650

Environment:
Communications Card

Cause:
Can a P765CA0A communications card for the ION 7550 / 7650 meter be used in an older ION 7500 / 7600?

Resolution:
The P765CA0A is backward compatible and will work on legacy ION 7500 / 7600 meters. There is a backup battery soldered to the board on the communications card, however only the ION 7550 / 7650 meters can utilize this additional backup battery.