{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
SQL Server 2005 Reporting Services Service will not start.

Goals and Symptoms

After the ION Enterprise v6.0 installation, SQL Server 2005 Reporting Services Service will not start. Since the reporting services service will not start, the web reporter feature will not install.

Causes and Fixes

To resolve this problem do the following:
1) Select ASP.NET as the default .NET Runtime for the default website (Right click default website > properties > asp.net tab > select asp.net 2.0 in the dropdown
2) Repair .NET Framework 3.5 SP1 from Add/Remove programs
3) Start SQL Reporting Services service
4) Run RSConfiguration Wizard from the ...\ION Enterprise\system\bin directory
5) Run modify from add/remove programs on ION Enterprise

Attachments

(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/f58ad94f085e467ec12577450010c09d/fl_block_5/0.1A60?OpenElement&FieldElemFormat=gif)
Date Created: June 11, 2010
Last Revised:
Public
Original Author: MN
All content © 1992-2010 Schneider Electric


Legacy KB System (APS) Data: RESL202645 V1.0, Originally authored by LaAd on 06/17/2010, Last Edited by LaAd on 06/17/2010
Related ranges: ION Enterprise V6.0

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.