Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the part numbers for the Current Transformers (CTs) used with the E4833?

Issue
Part numbers for current transformers (CTs) used with E4833 meter

Product Line
E4833

Environment
Current transformer (CTs)

Resolution
The E4833 is the 1/3 volt model of the E4800. Part numbers with associated descriptions are below:

ECT075050SC: 50A .333V Split Core Current Transformer with 0.75" Window Size
ECT075100SC: 100A .333V Split Core Current Transformer with 0.75" Window Size
ECT075150SC: 150A .333V Split Core Current Transformer with 0.75" Window Size
ECT075200SC: 200A .333V Split Core Current Transformer with 0.75" Window Size
ECT125100SC: 100A .333V Split Core Current Transformer with 1.25" Window Size
ECT125150SC: 150A .333V Split Core Current Transformer with 1.25" Window Size
ECT125200SC: 200A .333V Split Core Current Transformer with 1.25" Window Size
ECT125400SC: 400A .333V Split Core Current Transformer with 1.25" Window Size
ECT200200SC: 200A .333V Split Core Current Transformer with 2.00" Window Size
ECT200400SC: 400A .333V Split Core Current Transformer with 2.00" Window Size
ECT200600SC: 600A .333V Split Core Current Transformer with 2.00" Window Size
ECT300600SC: 600A .333V Split Core Current Transformer with 3" x 5" Window Size
ECT300800SC: 800A .333V Split Core Current Transformer with 3" x 5" Window Size