Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Trimming a database with Database Manager may give the error "Event Log File is full".

Goals and Symptoms

This is a Windows Application Event. It can happen in Windows XP, Windows Vista and perhaps other Windows operating systems.
After trimming or archiving a database, the following error may show up:
"The following error occurred: The event log file is full"

Causes and Fixes

It can be fixed by changing the Application Event Log properties:
- Right click My Computer > Manage > Event Viewer
- Right click Application Events > Properties
- In the Log size setting, change the setting to "Overwrite events as needed"
- Some postings on Google also suggest increase the Maximum log size, but it may not be necessary.


Legacy KB System (APS) Data: RESL204954 V1.0, Originally authored by KBAdPM on 03/29/2011, Last Edited by KBAdPM on 03/29/2011
Related ranges: ION Enterprise V6.0, ION Enterprise V5.6