Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ION8400 Meter Template Files

Product Line
ION8400

Environment
Templates

Resolution
You can install meter templates using ION Setup, ION Enterprise, StruxureWare Power Monitoring or Power Monitoring Expert. See the "Upgrading ION Device Firmware" technical note for complete details.

Install Templates with ION Setup

  1. Download the device template and save it to your ION Setup TEMPLATE folder (select the file below that matches your meter's feature set).

Use these .DCF files with ION Setup to perform firmware upgrades. These are default meter templates only. If you have custom programming in your meter, create your own template file before performing the firmware upgrade.

  1. Follow the upgrade procedures outlined in the Upgrading ION Device Firmware technical note.
See the .zip below for the following templates:
text
Version
text
Low Current
(Class 2)
text
Standard
(Class 20)
text
V264-265
text
8400_FAC-9S-39S-36S-76S_V2.6.0.0.9

8400_FAC-35S_V2.6.0.0.9

text
V262
text
8400_FAC-9S-39S-36S-76S_V2.6.0.0.2

8400_FAC-35S_V2.6.0.0.2

text
V244
text
8400_v240_FAC-C2A-9S-39S_V1.8.0.0.0

8400_v240_FAC-C2A-35S_V1.8.0.0.1

8400_v240_FAC-C2A-36S-76S_V1.8.0.0.0

text
8400_v240_FAC-9S-39S_V1.8.0.0.0

8400_v240_FAC-35S_V1.8.0.0.1

8400_v240_FAC-36S-76S_V1.8.0.0.0

Schneider Electric Saudi Arabia

Attachment(s)
8400_Templates.zip [640.6 KB]