Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the details for the Remote Display that is supported with EM4800 meters?

Issue
Clarify which EM4800 meters support the remote display and provide details about part numbers and installation requirements.

Product Line
EM4800 Series

Environment
Remote display operation with EM4800 meters.

Cause
The remote display is supported only on EM4800 meters that include the remote display port. Meters with part numbers in the format METxxEM48xx... have this port, while meters with part numbers in the format E48xx...SQD do not.

Resolution

  • The remote display will operate with EM4800 meters that have part numbers in the format:
    METxxEM48xx...
  • The remote display is not supported with meters that have part numbers in the format:
    E48xx...SQD
  • Reason: METxxEM48xx... meters include the remote display port required for operation.

Cutout Size:

  • The remote display uses a 92 x 92 mm cutout.

Part Numbers for Remote Display:

  • METSQEM48RD – EM4800 remote display, includes communications cable, Square D branded
  • METSEEM48RD – EM4800 remote display, includes communications cable, Schneider Electric branded

Functionality:

  • The remote display provides all measurements available on the onboard display.

Additional Information:

  • Sample picture only, showing form factor. Screen shown may not be available for EM4800 meters.
  • Front panel view included in original documentation.



Front panel

Legacy KB System (APS) Data:

  • RESL205819 V1.0
  • Originally authored by DaMi on 07/23/2011
  • Last Edited by DaMi on 07/23/2011

Related Ranges:

  • EM4800