Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
EGX300 Firmware Version History and Download Information

Issue:
Need to know the latest firmware upgrade available for the EGX300 and the features released with each upgrade.

Product Line:
EGX300

Environment:
EGX300 firmware upgrade

Cause:

The EGX300 periodically receives firmware updates that introduce new features, improvements, and bug fixes. Users may need this information for maintenance, compatibility, or troubleshooting purposes.



Resolution:
See attached file for update history, as January 2026.

Follow link below for EGX300 firmware download:
EGX300 v4.461 Firmware and 4.460 Disk Update | Schneider Electric

Schneider Electric Saudi Arabia

Attachment(s)
Public EGX300 Firmware Revision History.pdf [170.73 KB]