Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: Can the data points from a waveform capture be imported into excel from ION, SPM, or PME?

Product Line
Power Monitoring Expert 8.x
Power Monitoring Expert 7.x.x
Struxureware Power Monitoring 7.0.1
ION Enterprise


Cause
User would like to view the data points from a  waveform capture using PME, SPM, or ION

Resolution

1
1. Open the waveforms in the Vista Diagram for the meter.
2. Highlight the value to be plotted and click the "plot" button in the toolbar.
3. Right click on the plotted Waveform and select V1 --> Data (other values selected will be labeled accordingly e.g. V2, V3, I1, etc...)
4. Select all the data points and click the Copy button and Paste into Excel.

Please see the following video for walk through instructions.