Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the PM8ECC or the CM4ECC (ECC21) support BACnet?

Issue
User wants to know if PM8ECC or the CM4ECC (ECC21) supports BACnet

Product Line
PM8ECC
ECC21

Environment
BACnet communication

Resolution
The PM8ECC and the CM4ECC do not support BACnet. The only protocol supported with the ECC's is Modbus TCP/IP and on the serial side, ModusRTU, JBus, and Symax.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre