Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you send Input/Output links to the back in Designer (ION/SPM/PME)?

Issue
How do you send Input/Output links to the back in Designer (ION/SPM/PME)?

Product Line

ION Enterprise 6.0.x

Struxureware Power Monitoring 7.0.x (SPM 7.0.x)

Power Monitoring Expert 7.2.x (PME 7.2.x)

Power Monitoring Expert 8.x (PME 8)

Power Monitoring Expert 9.x (PME 9)

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024


Environment
Designer Module view of Input/Output Linkage

Cause
Links are in front of diagram objects and they want to be moved to make it easier to see the objects

Resolution
When working in Designer you can press Ctrl+B to send all links to the back.

Below are examples of before and after sending the links to the back:

Designer workspace with links shown in front of the modules

Designer workspace with links shown behind the modules