Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you replace the backlight in the Magelis XBTG2120, XBTG2130 or XBTG2220 using the XBTZG12 replacement?

Issue
How do you replace the backlight in the Magelis XBTG2120, XBTG2130 or XBTG2220 using the XBTZG12 replacement?

Product Line
Magelis XBTG Series

Environment
Physical HMI

Resolution
Attached in the "XBTZG12_replacement_backlight.zip" file you will find the procedure for replacing the backlight.
"XBTZG12 replacement backlight.pdf" is contained inside the zip.

Schneider Electric Saudi Arabia

Attachment(s)
XBTZG12_replacement_backlight.zip [1.27 MB]