Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum pending request supported by the TSXETG1000 TCP/IP/Modbus gateway?

Only one exchange can be made at a time: if the module is waiting for a response from the device, it cannot send a request. TCP requests
are suspended on the network (a maximum of 128 pending requests).