Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you adjust the grid spacing in Vijeo Designer?

Issue:
Adjusting the grid spacing in Vijeo Designer


Product Line:
Vijeo Designer


Resolution:
In the Property Inspector field for Graphical Panels you can adjust the GridXSpacing and GridYSpacing.
image1

    • GridXSpacing defines the amount of spaces (shown in dots) for the horizontal grid.
      GridYSpacing defines the amount of spaces (shown in dots) for the vertical grid.
      When setting these properties, use a value between 1 and the Maximum. The Maximum is one-half of the height
      defined in the Panel Size for the target machine. For example, if you select SVGA 800 x 600 in the Panel Size field,
      the value of the Maximum is 300 (Y) and 400 (X).