Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I scale or do a math calculation on a numeric display and also allow input using Vijeo Designer?

Issue:

How do I scale or do a math calculation on a numeric display and also allow input using Vijeo Designer?

Product:

Vijeo Designer

Resolution:

In Vijeo Designer, by default, if you do any math calculations in the variable field it will deactivate the "Enable Input Mode".
The solution would be:

1) Create a numeric display with input mode enabled. Let s call this NumericDisplay01. Assign it to INT01 variable for example.

2) Create another numeric display (NumericDisplay02) but with input mode disabled. For this one you would enter the expression (e.g. INT01*2) in the Variable field.

3) Overlay NumericDisplay02 on NumericDisplay01.

In Runtime, touch input will automatically go to NumericDisplay01 since it is disabled for NumericDisplay02.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)