Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to reset an ION 8600/8650 Front Panel Password

Issue
Need to reset an ION 8600/8650 Front Panel Password

Product Line
ION 8600
ION 8650 (v400 and v420 or later)

Environment
ION 86xx Meters - front panel

Cause
Front panel password of the meter has been forgotten or for other reasons needs to be reset to the factory default.

Resolution
Check to see that the meter has no Seal. This is a locking ring that attaches the clear plastic outer casing to the meter base. If there is a seal it will likely need to be re-sealed.

  1. Remove the front panel by holding the plastic casing and turning it 1/4 turn counter clockwise.
  2. Put the meter in "Test Mode" by pressing the Test button (uncovered by removing the plastic case)
  3. Hold down the ALT/Enter and Demand reset buttons together for 2-3 seconds
  4. A confirmation screen saying "Password Reset - Password reset to default" should appear.
  • 1
NOTE: ION 8650 version must be v400 or v420 or later