Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find fuse or circuit breaker info to protect an ATS48 soft starters?

Issue:
ATS48 circuit fuse or circuit breaker data.

Product Line:
Altistart ATS48

Environment:
ATS48

Cause:
Fuse or Circuit breaker protection for the ATS48 soft starter.

Resolution:
Refer to the ATS48 Installation Manual, which includes this table:

protection

For IEC ratings see the charts starting on page 15 using the page link below or attached document.
https://www.se.com/us/en/download/document/DIA2ED2140604EN/

Schneider Electric Saudi Arabia

Attachment(s)
ATS48 Catalog October 2014.pdf [3.79 MB]