Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the default values logged in the EGX400 and EGX200?

Issue
What values are logged by default from EGX200 or EGX400?

Product Line
EGX400
EGX200

Environment
Onboard Logging

Resolution
NOTE: The EGX200 does not have device logging.

The EGX400 ships from the factory with device profiles for standard Schneider Electric monitoring and protective devices.

Click the following link: EGX200/400 User's Guide | Schneider Electric , and refer to page 3 under "EGX400 Device List" for a list of supported devices and logged data.

Real energy, reactive energy, and apparent energy are logged by default for Schneider Electric Monitoring devices. For example, the EGX400 logs Real Energy and Real Power Demand for the Enercept and Energy Meter.

The EGX400 can log data at predefined intervals from up to 32 serially connected devices. For details, see "Device Logging" on page 5 and “Interval Data Logging (EGX400)” on page 13 of User guide.

NOTE: The Series 200 Power Meter (PM210) is not a loggable device type in the EGX400 with firmware v5.6. A device type template (.plt) file will be created at a later date. A temporarily work around is to select the PM700 device type for the PM200 meter and then enable logging. The PM700 and the PM200 share some of the same registers. Some PM700 quantities may not be applicable for the PM200.

Schneider Electric Saudi Arabia

Attachment(s)
EGX200_EGX400 User Guide.pdf [1.13 MB]